This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: SPI communication with EtherCAT - LAN9252

Part Number: TMS320F28335

Hi team,

Here's an issue from the customer may need your help:

Now the customer is working on the SPI communication between 28335 and EtherCAT -- LAN9252. The error reported on TwinCAT is as follows: the board of LAN9252 was self-welded. Also, does the PORT0 of EtherCAT slave station have to be the input port? They connected PORT1 to the computer, ESI file was burned successfully, and TwinCAT was able to scan the slave station information. So what's the problem?

Could you help check this case? Thanks.

Best Regards,

Cherry