Part Number: TMS320F2810
Other Parts Discussed in Thread: CODECOMPOSER, UNIFLASH,
Hi there,
I try to program a TMS320F2810 using Blackhawk USB560 v2 SystemTrace Debug probe and TI Uniflash or CodeComposer Studio.
In CCS, I installed the Blackhawk drivers (which work well with another Target controller). For uniflash, i installed the Blackhawk package provided here: https://www.blackhawk-dsp.com/support/uniflashv5
The debugger is recognized correctly by both - CCS and Uniflash. I use the standard settings from TMS320F2810 target config:

Unfortunately, when I try to connect the target, CCS gives the following error message to me:
Error connecting to the target: (Error -183 @ 0x0) The controller has detected a cable break far-from itself. The user must connect the cable/pod to the target. (Emulation package 9.3.0.00058)
I know this error message, I saw it sometimes when I forgot to connect the debug probe to the target. But it is all connected well.
Furthermore, when I try flashing the chip using XDS110 debug probe (using exactly the same wiring and the XDS110 default target config), it works well.
Do you have another idea where to look for the error next? Unfortunately, I am no JTAG-Guru ;)
Best regards,
Chris