Part Number: TMS320F280049
Other Parts Discussed in Thread: PMP22650, STRIKE
In PMP22650 description, it's described to be a GaN based bi-directional OBC application. But why is there a rectifier in PFC stage?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
Other Parts Discussed in Thread: PMP22650, STRIKE
In PMP22650 description, it's described to be a GaN based bi-directional OBC application. But why is there a rectifier in PFC stage?

Yes, this is fully bi-directional. The design operates normally without the rectifier in place. The rectifier was added due to learnings from previous designs to help with surge and lightning strike testing. During those tests it is not uncommon to see many hundred of amps which would have otherwise all been routed though the FET.
Regards,
Cody
Rookie,
Please not that these legs share the same gate drive input. This is because they doubled to allow more current carrying capacity.
Those are the low-frequency FETs, and are not two totem pole legs, I hope that this is now makes sense being that they share a gate drive input.
The high-frequency FETs are on another schematic page.
Regards,
Cody