Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMS320F28069M
Hi, I am trying to read ADC with TMS320f28379D launchpad. I am testing ADC channels by connecting potentiometers JP1, JP2, JP3, JP4, JP5 ON - JP6 OFF and connected to PC via USB. With the help of the MAtlab Simulink scope, I can see the bit changes without any problems. But in the case of JP1, JP2, JP3 OFF - JP4, JP5 ON- JP6 OFF, when I feed 3.3 V to J1 connector and GND to J2 connector and connect the potentiometer to the ADC channels, I can't see the bit changes. When I do the above experiments with the TMS320f28069M launchpad, I can read the ADC channels without any problems in both cases. What could be the reason for this? Thanks in advance.