I get this error message when I debug.
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error.
I uninstalled the driver and then rebooted as from what I have read that may fix problems. Either way the version is 2.0.0.2.
The error message calls out XDS100 but the device driver on the ports page lists XDS110. Could that make a difference?
I have also read that the speed setting may be wrong in target config but I see no option to adjust speed under advanced settings.
Thanks,
JH