Hi
I have a project that just uses a few global variables, but when I use CCS v11.2.0.00007 to compile it, I got a link error as follows:
<Linking>
"../F280049_RAM_lnk.cmd", line 41: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".econst" size 0x3378 page 1. Available memory ranges:
RAMDCPU size: 0x2000 unused: 0x1e20 max hole: 0x1e20
error #10010: errors encountered during linking; "Test_Comparator_Out2.out" not built
The linker shows there are 0x3378 words in .econst section, that's impossible.
My project is uploaded for your review.
Test Comparator Out2 (C code).zip
Thanks,
Jiakai