Other Parts Discussed in Thread: AMC3336, AMC3336-Q1, TMS320F28377D
Dear Sir,
"Sorry, I cannot find my previous post in forum, repost again"
As I am designing High Voltage DC-Link measurement, I have not enough pulse generator for AMC3336.
So, I want to use external pulse oscillator generator at 20MHz to supply CLKIN of AMC3336.
After that, I wan to tuse SDFM (eCAP_CH-04) to measure this voltage.
Would it be applicable for such circuit design ?
And I read that AMC3336 will output 128-bit stream at 10% duty when -1V and 90% duty at +1V.
In such above case, Will SDFM module can work with prior knowing the CLKIN 20Mhz but not knowing the begining of measurement bit ?
Best regards,
Narudol T.