Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
if i use flash mode, bootloader code is placed into RAM, how can i exit boot. there are two demos(SCIA or CAN in c2000ware) about flash, both use ram mode, initboot is the entry point of program,
in this assemble program, using LCR to call "main" function and end with LRETR, if the program boot from flash, how can i turn to the entry point.
_InitBoot:
; Initalize the stack pointer.
__stack: .usect ".stack",0
MOV SP, #__stack ; Initalize the stack pointer
; Initalize the device for running in C28x mode.
C28OBJ ; Select C28x object mode
C28ADDR ; Select C27x/C28x addressing
C28MAP ; Set blocks M0/M1 for C28x mode
CLRC PAGE0 ; Always use stack addressing mode
MOVW DP,#0 ; Initialize DP to point to the low 64 K
CLRC OVM
; Set PM shift of 0
SPM 0
; Decide which boot mode to use
LCR _main
; Cleanup and exit. At this point the EntryAddr
; is located in the ACC register
BF _ExitBoot,UNC
;-----------------------------------------------
; _ExitBoot
;-----------------------------------------------
;-----------------------------------------------
;This module cleans up after the boot loader
;
; 1) Make sure the stack is deallocated.
; SP = 0x400 after exiting the boot
; loader
; 2) Push 0 onto the stack so RPC will be
; 0 after using LRETR to jump to the
; entry point
; 2) Load RPC with the entry point
; 3) Clear all XARn registers
; 4) Clear ACC, P and XT registers
; 5) LRETR - this will also clear the RPC
; register since 0 was on the stack
;-----------------------------------------------
_ExitBoot:
;-----------------------------------------------
; Insure that the stack is deallocated
;-----------------------------------------------
MOV SP,#__stack
;-----------------------------------------------
; Clear the bottom of the stack. This will endup
; in RPC when we are finished
;-----------------------------------------------
MOV *SP++,#0
MOV *SP++,#0
;-----------------------------------------------
; Load RPC with the entry point as determined
; by the boot mode. This address will be returned
; in the ACC register.
;-----------------------------------------------
PUSH ACC
POP RPC
;-----------------------------------------------
; Put registers back in their reset state.
;
; Clear all the XARn, ACC, XT, and P and DP
; registers
;
; NOTE: Leave the device in C28x operating mode
; (OBJMODE = 1, AMODE = 0)
;-----------------------------------------------
ZAPA
MOVL XT,ACC
MOVZ AR0,AL
MOVZ AR1,AL
MOVZ AR2,AL
MOVZ AR3,AL
MOVZ AR4,AL
MOVZ AR5,AL
MOVZ AR6,AL
MOVZ AR7,AL
MOVW DP, #0
;------------------------------------------------
; Restore ST0 and ST1. Note OBJMODE is
; the only bit not restored to its reset state.
; OBJMODE is left set for C28x object operating
; mode.
;
; ST0 = 0x0000 ST1 = 0x0A0B
; 15:10 OVC = 0 15:13 ARP = 0
; 9: 7 PM = 0 12 XF = 0
; 6 V = 0 11 M0M1MAP = 1
; 5 N = 0 10 reserved
; 4 Z = 0 9 OBJMODE = 1
; 3 C = 0 8 AMODE = 0
; 2 TC = 0 7 IDLESTAT = 0
; 1 OVM = 0 6 EALLOW = 0
; 0 SXM = 0 5 LOOP = 0
; 4 SPA = 0
; 3 VMAP = 1
; 2 PAGE0 = 0
; 1 DBGM = 1
; 0 INTM = 1
;-----------------------------------------------
MOV *SP++,#0
MOV *SP++,#0x0A0B
POP ST1
POP ST0
;------------------------------------------------
; Jump to the EntryAddr as defined by the
; boot mode selected and continue execution
;-----------------------------------------------
LRETR