Part Number: LAUNCHXL-F28379D
All of the signals that I want to measure are max 3.3V.
JP6 can of course connect 5V to VREF. If I use this, do I go with the 3.3V max, and a "full-scale reading" corresponds to 3.3V, and I lose the resolution of values above this?
Or on the LaunchXL, is it possible to leave JP6 disconnected, and then jumper 3.3V to 5V somewhere else on the board? Such as closing JP5, and then putting a header from J5-1 (3.3V) to J7-1 (5V). So that the full 12-bit range will be used?
Thanks!