Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am trying to connect a Bluetooth module through SCI, the code worked well for CPU1, but when I tried to built it on cpu2 it is not working because of the following error:
Description Resource Path Location Type
<a href="file:/C:/ti/ccs1031/ccs/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment/blocking fails for section ".ebss" size 0x7a1c page 1. Available memory ranges: .ccsproject /Bluetooth-SCI_CPU2 line 57, external location: C:\ti\C2000Ware_4_00_00_00\device_support\f2837xd\common\cmd\2837xD_RAM_lnk_cpu2.cmd C/C++ Problem
I tried to increase the available memory
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x0000A2, length = 0x00035E
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
//RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
// RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000A0 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
.text : >>RAMD0 | RAMLS0 | RAMLS1 | RAMLS3, PAGE = 0
.cinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
#if defined(__TI_EABI__)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS3, PAGE = 0
.init_array : > RAMM0, PAGE = 0
.const : > RAMLS5, PAGE = 1
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
#else
.pinit : > RAMM0, PAGE = 0
.ebss : > RAMLS2 | RAMLS4 | RAMLS5 | RAMGS12 | RAMGS13 | RAMGS14 | RAMGS15, PAGE = 1
.econst : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
#endif
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} > RAMM0, PAGE = 0
#else
ramfuncs : > RAMM0 PAGE = 0
#endif
#endif
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
but still have the same error.
I am trying to link CPU1 and CPU2 as I need to read the data from an IMU using I2C controlled by CPU1 and send the data from CPU1 to CPU2 by IPC then send the data from CPU2 using Bluetooth to a mobile app. I will attach both codes. the first is the IMU code
#include "F28x_Project.h"
#include <math.h>
//#include"KF.h"
#include "UKF_IMU.h"
#define I2C_SLAVE_ADDR 0x68
#define I2C_NUMBYTES1 2
#define I2C_NUMBYTES2 1
#define MPU6050_ADDRESS 0x00D0
#define MPU6050_RA_SMPLRT_DIV 0x0019
#define MPU6050_RA_CONFIG 0x001A
#define MPU6050_RA_GYRO_CONFIG 0x001B
#define MPU6050_RA_ACCEL_CONFIG 0x001C
#define MPU6050_RA_FF_THR 0x001D
#define MPU6050_RA_FF_DUR 0x001E
#define MPU6050_RA_MOT_THR 0x001F
#define MPU6050_RA_MOT_DUR 0x0020
#define MPU6050_RA_ZRMOT_THR 0x0021
#define MPU6050_RA_ZRMOT_DUR 0x0022
#define MPU6050_RA_FIFO_EN 0x0023
#define MPU6050_RA_I2C_MST_CTRL 0x0024
#define MPU6050_RA_I2C_MST_STATUS 0x0036
#define MPU6050_RA_INT_PIN_CFG 0x0037
#define MPU6050_RA_INT_ENABLE 0x0038
#define MPU6050_RA_DMP_INT_STATUS 0x0039
#define MPU6050_RA_INT_STATUS 0x003A
#define MPU6050_RA_ACCEL_XOUT_H 0x003B
#define MPU6050_RA_ACCEL_XOUT_L 0x003C
#define MPU6050_RA_ACCEL_YOUT_H 0x003D
#define MPU6050_RA_ACCEL_YOUT_L 0x003E
#define MPU6050_RA_ACCEL_ZOUT_H 0x003F
#define MPU6050_RA_ACCEL_ZOUT_L 0x0040
#define MPU6050_RA_TEMP_OUT_H 0x0041
#define MPU6050_RA_TEMP_OUT_L 0x0042
#define MPU6050_RA_GYRO_XOUT_H 0x0043
#define MPU6050_RA_GYRO_XOUT_L 0x0044
#define MPU6050_RA_GYRO_YOUT_H 0x0045
#define MPU6050_RA_GYRO_YOUT_L 0x0046
#define MPU6050_RA_GYRO_ZOUT_H 0x0047
#define MPU6050_RA_GYRO_ZOUT_L 0x0048
#define MPU6050_RA_USER_CTRL 0x006A
#define MPU6050_RA_PWR_MGMT_1 0x006B
#define MPU6050_RA_PWR_MGMT_2 0x006C
#define MPU6050_RA_BANK_SEL 0x006D
#define MPU6050_RA_MEM_START_ADDR 0x006E
#define MPU6050_RA_MEM_R_W 0x006F
#define MPU6050_RA_DMP_CFG_1 0x0070
#define MPU6050_RA_DMP_CFG_2 0x0071
//#define RESTRICT_PITCH
#define DEG_RAD 0.017453292
void Ini_I2C (void);
void Ini_timer0(void);
void Ini_timer1(void);
void ACC_A(double x_dd, double y_dd, double z_dd);
__interrupt void timer1_isr(void);
__interrupt void i2c_int1a_isr(void);
__interrupt void IPPC0_ISR(void); // interrupt function to store data
Uint16 FailCount;
Uint16 IntSource,Ind;
//
// Function Prototypes
//
struct I2CMsgIn {
Uint16 mode;
Uint16 device_ADDR;
Uint16 NUMBYTES;
Uint16 sensor_Reg;
//Uint16 sensor_XOUT_L;
int16 MsgBuffer[12];
};
struct I2CMsgOut {
Uint16 mode;
Uint16 device_ADDR;
Uint16 NUMBYTES;
Uint16 MPU6050_RA;
Uint16 outMsg;
};
struct I2CMsgIn *CurrentMsgPtr;
struct I2CMsgOut *CurrentMsgPtrW;
Uint16 I2cb_WriteData(struct I2CMsgOut *msg);
Uint16 I2cb_ReadData(struct I2CMsgIn *msg);
int i,j,k,k1,k2,k3,k4,k5,a,f;
double dx,dy,dz,accX,accY,accZ;
double dx_f,dy_f,dz_f,accX_f,accY_f,accZ_f,tt,ts;
double in_buffer[6][20];
double temp1,temp2,temp3,temp4,temp5,temp6;
double roll,pitch,KF_roll,KF_pitch,AR;
int GGG;
UKF R_UKF,P_UKF;
void main(void)
{
struct I2CMsgIn I2C_Msgin;
struct I2CMsgOut I2C_Msgout;
I2C_Msgin.device_ADDR=0x68;
I2C_Msgin.NUMBYTES=1;
I2C_Msgout.device_ADDR=0x68;
I2C_Msgout.NUMBYTES=2;
//
EALLOW;
DevCfgRegs.CPUSEL5.bit.SCI_B =1;
EDIS;
InitSysCtrl();
InitGpio();
GPIO_SetupPinMux(19, GPIO_MUX_CPU2, 2);
GPIO_SetupPinOptions(19, GPIO_INPUT, GPIO_PUSHPULL);
GPIO_SetupPinMux(18, GPIO_MUX_CPU2, 2);
GPIO_SetupPinOptions(18, GPIO_OUTPUT, GPIO_ASYNC);
DINT;
InitPieCtrl();
//clear IPC flags
IpcRegs.IPCCLR.all= 0xFFFFFFFF;
//enable IPC PIE Interrupts
EALLOW;
PieVectTable.IPC0_INT = &IPPC0_ISR;
EDIS;
PieCtrlRegs.PIEIER1.bit.INTx13= 1;
IER |= 0x0001;
IpcRegs.IPCCLR.bit.IPC0= 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
//wait here until CPU2 is ready
while(IpcRegs.IPCSTS.bit.IPC17 ==0)
IpcRegs.IPCACK.bit.IPC17 =1;
IFR=0x0000;
InitPieVectTable();
EALLOW;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
IER |= M_INT1;
EINT;
EDIS;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.I2CB_INT = &i2c_int1a_isr;//assign interrupt function of I2cb
EDIS; // This is needed to disable write to EALLOW protected registers
// Enable I2C __interrupt 1 in the PIE: Group 8 __interrupt 1
//
PieCtrlRegs.PIEIER8.bit.INTx3 = 1;
//
// Enable CPU INT8 which is connected to PIE group 8
//
IER |= M_INT8;
EINT;
Ini_I2C();
Ini_timer0();
CurrentMsgPtrW= &I2C_Msgout;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->MPU6050_RA= MPU6050_RA_USER_CTRL;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x00;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
//I2cbRegs.I2CMDR.bit.STP=0;
//I2cbRegs.I2CSTR.bit.BB=0;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->MPU6050_RA=MPU6050_RA_PWR_MGMT_1;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x01;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
//I2cbRegs.I2CMDR.bit.STP=0;
//I2cbRegs.I2CSTR.bit.BB=0;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->MPU6050_RA= MPU6050_RA_INT_PIN_CFG;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x02;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
// I2cbRegs.I2CMDR.bit.STP=0;
// I2cbRegs.I2CSTR.bit.BB=0;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->device_ADDR=I2C_SLAVE_ADDR;
CurrentMsgPtrW->MPU6050_RA= MPU6050_RA_SMPLRT_DIV;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x07;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
// I2cbRegs.I2CMDR.bit.STP=0;
// I2cbRegs.I2CSTR.bit.BB=0;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->MPU6050_RA= MPU6050_RA_CONFIG;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x06;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
//I2cbRegs.I2CMDR.bit.STP=0;
// I2cbRegs.I2CSTR.bit.BB=0;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->MPU6050_RA= MPU6050_RA_GYRO_CONFIG;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x00;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
// I2cbRegs.I2CMDR.bit.STP=0;
// I2cbRegs.I2CSTR.bit.BB=0;
CurrentMsgPtrW->mode = I2C_MSGSTAT_WRITE_BUSY;
CurrentMsgPtrW->MPU6050_RA= MPU6050_RA_ACCEL_CONFIG;
CurrentMsgPtrW->NUMBYTES=2;
CurrentMsgPtrW->outMsg=0x00;
FailCount= I2cb_WriteData(CurrentMsgPtrW);
while(I2cbRegs.I2CMDR.bit.STP==1);
I2cbRegs.I2CSTR.bit.XSMT=0;
//I2cbRegs.I2CMDR.bit.STP=0;
// I2cbRegs.I2CSTR.bit.BB=0;
// Clear incoming message buffer
for (i = 0; i < 12; i++)
{I2C_Msgin.MsgBuffer[i] = 0x0000;}
i=0;k=0;
CurrentMsgPtr->mode=I2C_MSGSTAT_SEND_NOSTOP;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_XOUT_H;
CpuTimer1Regs.TCR.bit.TRB=1;
CpuTimer1Regs.TCR.bit.TSS=0;
//R_UKF.setAngle(0.00); // First set roll starting angle
// P_UKF.setAngle(0.00); // Then pitch
//f=1;
while(1)
{
CpuTimer0Regs.TCR.bit.TRB=1;
CpuTimer0Regs.TIM.all=0xFFFFFFFF;
CpuTimer0Regs.TCR.bit.TSS=0;
tt= CpuTimer0Regs.TIM.all;
CurrentMsgPtrW->mode = I2C_MSGSTAT_INACTIVE;
CurrentMsgPtr= &I2C_Msgin;
CurrentMsgPtr->device_ADDR=I2C_SLAVE_ADDR;
CurrentMsgPtr->NUMBYTES=1;
while(f==1)
{
switch(i)
{
case 0:CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_XOUT_H;
f=0;
break;
case 1:CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_XOUT_L;
f=0;
break;
case 2: dx=((CurrentMsgPtr->MsgBuffer[0] << 8) | CurrentMsgPtr->MsgBuffer[1]);
dx=(dx/131)*DEG_RAD;
in_buffer[0][k]=dx;
f=0;
k=k+1;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_YOUT_H;
break;
case 3: CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_YOUT_L;
f=0;
break;
case 4: dy=((CurrentMsgPtr->MsgBuffer[2] << 8) | CurrentMsgPtr->MsgBuffer[3]);
dy=(dy/131)*DEG_RAD;
in_buffer[1][k1]=dy;
k1=k1+1;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_ZOUT_H;
f=0;
break;
case 5: CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_ZOUT_L;
f=0;
break;
case 6: dz=((CurrentMsgPtr->MsgBuffer[4] << 8) | CurrentMsgPtr->MsgBuffer[5]);
dz=(dz/131)*DEG_RAD;
in_buffer[2][k2]=dz;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_ACCEL_XOUT_H;
f=0;
k2=k2+1;
break;
case 7: CurrentMsgPtr->sensor_Reg=MPU6050_RA_ACCEL_XOUT_L;
f=0;
break;
case 8: accX=((CurrentMsgPtr->MsgBuffer[6] << 8) | CurrentMsgPtr->MsgBuffer[7]);
accX=accX;
in_buffer[3][k3]=accX;
k3=k3+1;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_ACCEL_YOUT_H;
f=0;
break;
case 9: CurrentMsgPtr->sensor_Reg=MPU6050_RA_ACCEL_YOUT_L;
f=0;
break;
case 10: accY=((CurrentMsgPtr->MsgBuffer[8] << 8) | CurrentMsgPtr->MsgBuffer[9]);
accY=accY;
in_buffer[4][k4]=accY;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_ACCEL_ZOUT_H;
f=0;
k4=k4+1;
break;
case 11: CurrentMsgPtr->sensor_Reg=MPU6050_RA_ACCEL_ZOUT_L;
f=0;
break;
case 12: accZ=((CurrentMsgPtr->MsgBuffer[10] << 8) | CurrentMsgPtr->MsgBuffer[11]);
accZ=accZ;
in_buffer[5][k5]=accZ;
CurrentMsgPtr->sensor_Reg=MPU6050_RA_GYRO_XOUT_H;
i=0;f=0;
k5=k5+1;
break;
}
}
if(a==1)
{CurrentMsgPtr->mode=I2cb_ReadData(CurrentMsgPtr);}
if(I2C_Msgout.mode == I2C_MSGSTAT_INACTIVE)
{
//
// Check incoming message status.
//
if(CurrentMsgPtr->mode == I2C_MSGSTAT_SEND_NOSTOP)
{
while(I2cb_ReadData(CurrentMsgPtr) != I2C_SUCCESS);
CurrentMsgPtr = &I2C_Msgin;
I2C_Msgin.mode = I2C_MSGSTAT_SEND_NOSTOP_BUSY;
}
//
//
else if(CurrentMsgPtr->mode == I2C_MSGSTAT_RESTART)
{
// Read data portion
while(I2cb_ReadData(CurrentMsgPtr) != I2C_SUCCESS);
}
}
//I2C_MSGSTAT_RESTART
//
CurrentMsgPtr->mode= I2C_MSGSTAT_RESTART;
for( j=0;j<20;j++)
{
temp1+=in_buffer[0][j];
temp2+=in_buffer[1][j];
temp3+=in_buffer[2][j];
temp4+=in_buffer[3][j];
temp5+=in_buffer[4][j];
temp6+=in_buffer[5][j];
}
dx_f=temp1/20;//0.006667
temp1=0;
dy_f=(temp2/20);//+0.148;
temp2=0;
dz_f=temp3/20;
temp3=0;
accX_f=temp4/20;
temp4=0;
accY_f=temp5/20;
temp5=0;
accZ_f=temp6/20;
temp6=0;
if(k>=20)
{k=0;}
if(k1>=20)
{k1=0;}
if(k2>=20)
{k2=0;}
if(k3>=20)
{k3=0;}
if(k4>=20)
{k4=0;}
if(k5>=20)
{k5=0;}
ACC_A(accX_f,accY_f,accZ_f);
// ACC_A(accX,accY,accZ);
if ((roll < -1.5708 && KF_roll > 1.5708) || (roll > 1.5708 && KF_roll < -1.5708))
{
//kalmanX.setAngle(roll);
R_UKF.setAngle(roll);
KF_roll = roll;
}
else
// KF_roll = kalmanX.getAngle(roll, dx_f, ts); // Calculate the angle using a Kalman filter
{ KF_roll=R_UKF.EstimatUKF(roll, dx_f, ts);
AR=KF_roll-0.72;
}
// if (abs(KF_roll) > 1.5708)
// { dy_f = -dy_f; }// Invert rate, so it fits the restricted accelerometer reading
// KF_pitch = P_UKF.EstimatUKF(pitch, dy_f, ts);
// f=0;
a=0;
ts= 0.00000001*(tt-CpuTimer0Regs.TIM.all);
}
}
void Ini_I2C()
{
EALLOW;
//J1 ....(9-10)I2C "GPIO 104 & 105" (blue 10)
GpioCtrlRegs.GPBGMUX1.bit.GPIO40=1;GpioCtrlRegs.GPBMUX1.bit.GPIO40=2;
GpioCtrlRegs.GPBGMUX1.bit.GPIO41=1;GpioCtrlRegs.GPBMUX1.bit.GPIO41=2;
GpioCtrlRegs.GPDPUD.bit.GPIO104 = 0;
GpioCtrlRegs.GPDPUD.bit.GPIO105 = 0;
I2cbRegs.I2CSAR.all = 0x68; // Slave address - MPU6050
I2cbRegs.I2CPSC.all = 15; // Prescaler - need 7-12 Mhz on module clk
I2cbRegs.I2CCLKL = 10; // NOTE: must be non zero 275 work for EKF
I2cbRegs.I2CCLKH = 5; // NOTE: must be non zero 5 work for EKF
I2cbRegs.I2CIER.all =0x24; // Enable SCD & ARDY __interrupts
I2cbRegs.I2CMDR.all = 0x0020; // Take I2C out of reset
// Stop I2C when suspended
I2cbRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO
I2cbRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT,
EDIS;
}
void Ini_timer0()
{
EALLOW; // This is needed to write to EALLOW protected registers
CpuSysRegs.PCLKCR0.bit.CPUTIMER0=1;
CpuTimer0Regs.TIM.all=0xFFFFFFFF;
CpuTimer0Regs.PRD.bit.LSW=0xFFFF;
CpuTimer0Regs.PRD.bit.MSW=0xFFFF;
CpuTimer0Regs.TCR.bit.TIE=0;
CpuTimer0Regs.TCR.bit.TIF=1;
CpuTimer0Regs.TCR.bit.TSS=0;
CpuTimer0Regs.TCR.bit.TRB=1;
CpuTimer0Regs.TCR.bit.FREE=1;
CpuTimer0Regs.TCR.bit.SOFT=0;
CpuTimer0Regs.TPR.bit.TDDR=0x00;
CpuTimer0Regs.TPR.bit.PSC=0x0000;
CpuTimer0Regs.TPRH.bit.TDDRH=0x00;
EDIS;
}
Uint16 I2cb_ReadData(struct I2CMsgIn *msg)
{
if(I2cbRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
if(msg->mode ==I2C_SUCCESS)
{
msg->mode = I2C_MSGSTAT_RESTART;
}
I2cbRegs.I2CSAR.all =msg->device_ADDR;
if(msg->mode == I2C_MSGSTAT_SEND_NOSTOP)
{
if(I2cbRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
I2cbRegs.I2CDXR.all =msg->sensor_Reg;
I2cbRegs.I2CMDR.all = 0x2620;
while(I2cbRegs.I2CMDR.bit.STP==1);
}
else if(msg->mode == I2C_MSGSTAT_RESTART)
{
I2cbRegs.I2CCNT = 1; // Setup how many bytes to expect
I2cbRegs.I2CMDR.all = 0x2C20; // Send restart as master receiver
}
return I2C_SUCCESS;
}
Uint16 I2cb_WriteData(struct I2CMsgOut *msg)
{
// Wait until the STP bit is cleared from any previous master communication.
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if(I2cbRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
//
// Setup slave address
//
I2cbRegs.I2CSAR.all = msg->device_ADDR;
//
// Check if bus busy
//
if(I2cbRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
I2cbRegs.I2CCNT =2;
I2cbRegs.I2CDXR.all = msg->MPU6050_RA;
I2cbRegs.I2CDXR.all =msg->outMsg;
//
// Send start as master transmitter
//
I2cbRegs.I2CMDR.all = 0x6E20;
return 0;
}
__interrupt void i2c_int1a_isr(void)
{
//
// Read __interrupt source
//
IntSource = I2cbRegs.I2CISRC.all;
if(IntSource == I2C_SCD_ISRC)
{
//
// If completed message was writing data, reset msg to inactive state
//
if(CurrentMsgPtrW->mode == I2C_MSGSTAT_WRITE_BUSY)
{
CurrentMsgPtrW->mode = I2C_MSGSTAT_INACTIVE;
}
else
{
CurrentMsgPtr->MsgBuffer[i]=I2cbRegs.I2CDRR.all;
i=i+1;
f=1;
// a=0;
}
}
else if(IntSource == I2C_ARDY_ISRC)
{
if(I2cbRegs.I2CSTR.bit.NACK == 1)
{
I2cbRegs.I2CMDR.bit.STP = 1;
I2cbRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
}
else if(CurrentMsgPtr->mode == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
{
CurrentMsgPtr->mode = I2C_MSGSTAT_RESTART;
}
}
else
{
//
// Generate some error due to invalid __interrupt source
//
__asm(" ESTOP0");
}
IpcRegs.IPCSENDDATA = (Uint32) KF_roll; //write the results to IPC data register
IpcRegs.IPCSET.bit.IPC1 =1;
//
// Enable future I2C (PIE Group 8) __interrupts
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP8;
}
__interrupt void IPPC0_ISR(void)
{
IpcRegs.IPCACK.bit.IPC0 =1; // clear IPC flag
GGG = (Uint16) IpcRegs.IPCRECVDATA; //read results
}
//
void ACC_A(double x_dd, double y_dd, double z_dd)
{
float ss;
roll = atan2(y_dd,-z_dd);
ss=pow(z_dd*z_dd + y_dd*y_dd,0.5);
// pitch = atan2(x_dd,sqrt(y_dd*y_dd + z_dd*z_dd))/DEG_RAD;
if (y_dd<0)
{
pitch=(atan(x_dd/-ss));
}
else
{
pitch=(atan(x_dd/ss));
}
//pitch=pitch/DEG_RAD;
}
this code is working well and I am able to read from the IMU.
the second code is the Bluetooth code which is not working
//
#include "F28x_Project.h"
#include "math.h"
#include <string.h>
#include <stdio.h>
//
// Global variable
//
float tt;
float ts;
int LoopCount;
float v=0;
int x=0;
char bb;
char *msg;
char *rdataB;
int gsample; // indicators to the send data
char *senddata; // char matrix will be used to send the data
// example data of the send gyro data
double roll[15600];
char msg1; //used to store the natural number
char msg2; // first decimal
char msg3; // second decimal
char msg4; // third decimal
Uint16 k=0; //counter for recived data inside the interrupt
Uint16 j=0; // counter to send the data inside the interrupt function
int i=0;
int z=0;
int t;
int counter;
//
// Function Prototypes
//
void Ini_timer0(void);
void scib_bluetooth_init(void); // initiate the SCI peripheral and sort its configurations
void scib_fifo_init(void); // also used to initiate the SCI peripheral
void scib_senddata(int a); // send one character
void scib_msg(char *msg); // used to send a group of characters
interrupt void scibReceiveIsr(void); // interrupt function to receive the command
__interrupt void IPPC1_ISR(void); // interrupt function to store data
//
// Main
//
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
InitSysCtrl();
//
//CPUSEL5
//
// Step 3. Clear all __interrupts and initialize PIE vector table:
// Disable CPU __interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE __interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU __interrupts and clear all CPU __interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
InitPieVectTable();
//clear IPC1 flag
IpcRegs.IPCCLR.bit.IPC1= 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
//enable ISR of SCIB
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.SCIB_RX_INT = &scibReceiveIsr;
PieVectTable.IPC1_INT = &IPPC1_ISR;
EDIS; // This is needed to disable write to EALLOW protected registers
// enable IPC PIE Interrupt
PieCtrlRegs.PIEIER1.bit.INTx14 =1;
IER |= 0x0001;
// let CPU1 know that CPU2 is ready
IpcRegs.IPCSET.bit.IPC17=1;
//
// Step 4. User specific code:
//
scib_fifo_init(); // Initialize the SCI FIFO
scib_bluetooth_init(); // Initialize SCI for bluetooth
Ini_timer0();
//
// Enable interrupts required for this example
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx3 = 1; // PIE Group 9, INT3
IER = 0x100; // Enable CPU INT
IER |= M_INT1;
EINT;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
for(;;)
{
ts= 0.00000001*(tt-CpuTimer0Regs.TIM.all);
CpuTimer0Regs.TCR.bit.TRB=1;
CpuTimer0Regs.TIM.all=0xFFFFFFFF;
CpuTimer0Regs.TCR.bit.TSS=0;
tt= CpuTimer0Regs.TIM.all;
t++;
if (x==1 || x==2)
{
//for (gsample=0; gsample <= 299;gsample++) // example vector to check the send data
//{
// v= sgyrodata[gsample];
if(x==1)
{
v= sin(t);
}
if (x==2)
{
v= sin(t)+0.5*cos(0.5*t)+0.2*sin(2*t);
}
//v=x;
int hundreds,tens,ones;
//
// define the sign of the send number
//
char sign;
if(v>=0)
{
sign = '0';
}
else
{
sign = '1';
v=-v;
}
int v1 = v; // get the natural number
float v2 = v-v1; // get the decimals
int t = v2*1000; // make the decimals as natural numbers to send
//
// separate the ones and tens and hundreds
//
ones= t%10;
tens= (t/10)%10;
hundreds= (t/100)%10;
//
// convert the integers to charecters
//
msg1= v1 + '0';
msg2= hundreds+ '0';
msg3= tens+ '0';
msg4= ones+ '0';
//
// create the vectror to send
//
/* senddata[0]='9';
senddata[1]='8';
senddata[2]='7'; */
senddata[0]='\r';
senddata[1]='\n';
senddata[2]= sign;
senddata[3]= msg1;
senddata[4]='.';
senddata[5]=msg2;
senddata[6]=msg3;
senddata[7]=msg4;
senddata[8]='\n';
// senddata[9]='\0';
// scib_msg(senddata); // sending the data
for(k=0;k<=9;k++)
{
scib_senddata(senddata[k]);
}
}
gsample=0;
}
// }
}
//
// scia_echoback_init - Test 1,SCIA DLB, 8-bit word, baud rate 0x000F,
// default, 1 STOP bit, no parity
//
void scib_bluetooth_init()
{
//
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function
//
ScibRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.bit.RXBKINTENA = 1;
ScibRegs.SCIFFRX.all = 0x2021;
//
// SCIA at 9600 baud
// @LSPCLK = 25 MHz (100 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x45.
//
ScibRegs.SCIHBAUD.all = 0x0001;
ScibRegs.SCILBAUD.all = 0x0045;
ScibRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset
}
//
// scib_xmit - Transmit a character from the SCI
//
void scib_senddata(int a)
{
while (ScibRegs.SCIFFTX.bit.TXFFST != 0) {}
ScibRegs.SCITXBUF.all =a;
}
//
// scia_msg - Transmit message via SCIA
//
void scib_msg(char * msg)
{
int i;
i = 0;
while(msg[i] != '\0')
{
scib_senddata(msg[i]);
i++;
}
}
//
// scia_fifo_init - Initialize the SCI FIFO
//
void scib_fifo_init()
{
ScibRegs.SCIFFTX.all = 0xE040;
ScibRegs.SCIFFRX.all = 0x2044;
ScibRegs.SCIFFCT.all = 0x0;
}
void Ini_timer0()
{
EALLOW; // This is needed to write to EALLOW protected registers
CpuSysRegs.PCLKCR0.bit.CPUTIMER0=1;
CpuTimer0Regs.TIM.all=0xFFFFFFFF;
CpuTimer0Regs.PRD.bit.LSW=0xFFFF;
CpuTimer0Regs.PRD.bit.MSW=0xFFFF;
CpuTimer0Regs.TCR.bit.TIE=0;
CpuTimer0Regs.TCR.bit.TIF=1;
CpuTimer0Regs.TCR.bit.TSS=0;
CpuTimer0Regs.TCR.bit.TRB=1;
CpuTimer0Regs.TCR.bit.FREE=1;
CpuTimer0Regs.TCR.bit.SOFT=0;
CpuTimer0Regs.TPR.bit.TDDR=0x00;
CpuTimer0Regs.TPR.bit.PSC=0x0000;
CpuTimer0Regs.TPRH.bit.TDDRH=0x00;
EDIS;
}
interrupt void scibReceiveIsr(void)
{
LoopCount++;
k++;
rdataB[k]=ScibRegs.SCIRXBUF.all; // Read data
/* while(j != 1)
{
scib_senddata(rdataB[j]);
j++;
}
j=0;*/
bb= (char)rdataB[k];
x= bb -'0';
z=x;
ScibRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
__interrupt void IPPC1_ISR(void)
{
IpcRegs.IPCACK.bit.IPC1 =1; // clear IPC flag
roll[counter] = (Uint16) IpcRegs.IPCRECVDATA; //read results
counter++;
if (counter>15600)
{counter =0;
IpcRegs.IPCSENDDATA = 777;
IpcRegs.IPCSET.bit.IPC0 = 1;
}
}
//
// End of file
//
regards
Hamza.