This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280048-Q1: SysConfig Editor for ADC

Part Number: TMS320F280048-Q1
Other Parts Discussed in Thread: SYSCONFIG

Hi,

I'm trying to configure the pins using SysConfig.

My ADC ports are  6,7,8 and 9 pins of mcu. However, I can only add 3 units of ADC and only configure 1 port for each ADC A, ADC B and ADC C in SysConfig editor. 

Pin 6: A6

Pin 7: B2,C6

Pin 8: B3

Pin 9: A2,B6

How can I achieve it?

Why can't I configure A2 and A6 at system config tool? How can I achieve it?

  • Why can't I configure A2 and A6 at system config tool? How can I achieve it?

    You can. For A2 and A6 you configure one ADC module (e.g. myADC0) but 2 SOCs (Start Of Conversions). Click the arrow in the 'SOC Configurations' box and begin adding your SOCs which, among other parameters, you choose the ADC channel or pin.