Part Number: TMS320F28335
Other Parts Discussed in Thread: LP2992
Hi TI
1. The customer's TMS320F28335 occasionally has a startup exception: from the phenomenon, it seems that the kernel is not up;
2. In case of abnormality, press the reset key to operate normally;
3. The 1.8V and 3.3V of the measured power supply are normal in case of problems;
4. For 600pcs of boards running on site, 5~10 boards will have this abnormality each time they are powered on, and the boards with problems are not fixed;
The customer did not consider the 1.8V and 3.3V power on sequence when designing the PCB. Because the customer uses LP2992 to convert 3.3V to 1.8V, 1.8V will lag behind the 3.3V power supply. Does TMS320F28335 have any restrictions on the order of 1.8V and 3.3V power supply? Please see the figure below for the customer's power supply design. Thank you.