Part Number: TMS320F28386S
I want to use GPIO57 as an output but the pin is not going high as it does when I use the same setup on a 28000049C. I see it is listed in SPRSP14D in table 6-7 as a muxed pin. Is there a default setting that must be overcome for it to be an I/O? Muxing seems to be a subject with somewhat of a learning curve and I have not found an answer yet in my search.
Thanks,
john
reset57()
{
Device_init();
Device_initGPIO();
Interrupt_initModule();
Interrupt_initVectorTable();
EINT;
ERTM;
GPIO_setPadConfig(57U, GPIO_PIN_TYPE_STD);
GPIO_setDirectionMode(57U, GPIO_DIR_MODE_OUT);
int i;
GPIO_writePin(57U, 0);
DEVICE_DELAY_US(50);
GPIO_writePin(57U, 1);
DEVICE_DELAY_US(50);
SysCtl_resetDevice();
return 0;
}