Part Number: TIDM-02000
Hi,
When using the C2000 in peak current mode control, is there a formula to determine the accuracy or resolution of the main output of the power supply based on DAC slope compensator and PWM frequency?
In another word, what is the main output total resolution for example when:
1) slope is 20, PWM freq = 100KHz
2) slope is 20, PWM freq = 200KHz
3) slope is 40, PWM freq = 200KHz
I try to understand how accurate the output can be based on the settings. I try to see if the TI solution can achieve a specific requirement.
Thanks for your help,
Arnaud