Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am developing my project with MCU F28388D, I used all 3 cores of MCU.
Everything is still ok when I build my 3 projects for 3 cores in debug mode (optimization lever: off. opt_for_speed :level 2).
But the problem occurs when I build them in release mode, detail:
CPU1 core: --opt_lever : o2, opt_for_speed: level2.
CPU2 core: --opt_lever : o2, opt_for_speed: level2.
CM core: --opt_lever : off, opt_for_speed: level2.
My complier for C28x: Ti v 18.12.4.LTS and arm core: Ti v18.12.4.LTS. C2000ware ver 3.02.00.00 inside the C2000ware_motorcontrol_SKD_3_00_01_00. CCS9.3.0.00012
The program is still running but there is a problem, I found that the failure when CPU2 read a variable from shared ram between CM core to CPU2 core (the same happen with CPU1 core).
The reading command i put in back-ground loop (while (1) in main loop:
ex code in CPU2 core
void main()
{
.......
while (1) // back ground loop
{
// reading a variable from share ram CM to CPU2
sysmode = ipcCMtoCPU2Data.systemMode; ===> failed
......
}
}
Temporary solution, I put the delay DEVICE_DELAY_US(10U) - about 10us before reading command : "sysmode = ipcCMtoCPU2Data.systemMode" or change the -opt_level -> off or change the opt_for_speed to level 1, the program runs ok.
But I don't know the root core reason, I thinks the problem relates about the accessing the shared ram between the CPU cores and the safety features to protect chip?
Can you give me the reason or information about this issue on some document like TRM, datasheet...?