Part Number: TMS320F28386S
In the F28386S is the UART controllable by the C28 or only the CM?
The reason I ask is that the project I am supporting wants to use software controlled firmware updates as per SPRACN1 but they also want to use RS-485 which has been connected via level shifters to UART-A. Sounds like a mess to me that would be much more easily implemented if the level shifters were connected to one of the SCI ports. Especially since the SPRACN1 application note is geared toward the C28.
Thanks,
John