Part Number: TMS320F280025C
Other Parts Discussed in Thread: USB2ANY, TCAN1145-Q1
Hello,
I am configuring TCAN for selective wake up with USB2ANY and I have connected vector device to send CAN wake up Frame in sleep mode.
I have below observations on the same;
Periodic RX error is observed on CAN if in standby or sleep mode.

No RX error observed in normal mode, but not able to send any message on CAN, seen below error on write window

what is missing here, and how should be the CAN wakeup frame structure?
Arb ID: 03 Data: 01 07 Is this correct, if I configure the same through SPI.