Other Parts Discussed in Thread: C2000WARE
Hi,
I am working on a project to upgrade the firmware of TMS320F28377D device from another device through USB. We do not want to use physical setting on the PINs to go to boot mode. When we use the asm(" LB 0x3fe868"); command, it seems the boot loader is activated (the product id changes to 00ff and TMS320F28377D shows up in the other device as Boot loader), is this right? do I just need now to send the two files (flash kernel and new image) to the TMS320F28377D device through USB?
Thanks,
Hossein.