Greetings! In the example labs as LAB06e usage of 2 motor is demonstrated. BUT the motors are connected on different adc and pwm channels - in short there are 2 inverters operating with single uC. In my case I have use a single inverter and there will be connected 2 motor. What functionality of InstaSPIN i can use in this case? Can I used it the same way as there is only 1 motor? Motor ID and so on?
Thanks!
PP: The motors with act simultaneously -> same direction same speed and so on. They move the bridge of a crane..