Part Number: TMS320F28386S
The code below is taken from flash_kernel_c28x_dual_ex1_sci_get_function_cpu1.c. I added the while loop that attempts to write and read.
The write puts "abc" on the com7 Putty terminal but the read never returns.
Suggestions please.
int32_t sciGetFunction(uint32_t BootMode)
{
uint32_t EntryAddr;
uint16_t command;
uint16_t data[10]; // 16*10 = 128 + 32
uint16_t length;
//
// Check if SCI is enabled or not
//
if(SysCtl_isPeripheralPresent(SYSCTL_PERIPH_PRESENT_SCIA) != 0x01)
{
return 0xFFFFFFFF;
}
//
// Assign GetWordData to the SCI-A version of the
// function. GetWordData is a pointer to a function.
//
getWordData = sciaGetWordData;
//
// Initialize the SCI-A port for communications
// with the host.
//
sciaInit(SCI_BOOT_ALT1);
char buf[128];
char buf2[128];
strcpy(buf, "abc");
while(1)
{
SCI_writeCharArray(SCIA_BASE, (uint16_t *) buf, strlen(buf));
DEVICE_DELAY_US(2000000U);
SCI_readCharArray(SCIA_BASE, (uint16_t *) buf2, 4);
DEVICE_DELAY_US(2000000U);
}
...
}
void sciaInit(uint32_t BootMode)
{
//
// Enable the SCI-A clocks
//
EALLOW;
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIA);
//
// TRM, 0x0007 -> scaler of 14. OSCLOK low speed scaling for SCI.
//
SysCtl_setLowSpeedClock(SYSCTL_LSPCLK_PRESCALE_4);
// reset SCI channels.
SCI_resetChannels(SCIA_BASE);
HWREGH(SCIA_BASE + SCI_O_FFTX) &= ~SCI_FFTX_TXFIFORESET;
//
// 1 stop bit, No parity, 8-bit character
// No loopback
//
// CLK speed and Baud rate get overwritten in autobaud_lock function later.
//
SCI_disableLoopback(SCIA_BASE);
SCI_setConfig(
SCIA_BASE, DEVICE_LSPCLK_FREQ, 9600U, //DEFAULT_BAUD,
SCI_CONFIG_WLEN_8 | SCI_CONFIG_STOP_ONE | SCI_CONFIG_PAR_NONE);
//
// Enable TX, RX, Use internal SCICLK
//
HWREGH(SCIA_BASE + SCI_O_CTL1) = (SCI_CTL1_TXENA | SCI_CTL1_RXENA);
//
// Disable RxErr, Sleep, TX Wake,
// Disable Rx Interrupt, Tx Interrupt
//
HWREGB(SCIA_BASE + SCI_O_CTL2) = 0x0U;
SCI_disableFIFO(SCIA_BASE);
//
// Relinquish SCI-A from reset
//
SCI_enableModule(SCIA_BASE);
EDIS;
GPIO_setMasterCore(84, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_84_SCIA_TX);
GPIO_setDirectionMode(84, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(84, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(84, GPIO_QUAL_ASYNC);
return;
}