Part Number: TMS320F280230
Dear TI engineers,
I have a doubt in my work about spi between 28337s and 280230 or 280270.
Normally, communication of spi work well like pic1 below.

But, it could also not work like pic2 blow.

When fault happened, the SPIFFTX.BIT.TXFFST would be 4 which is the max value. So, data could not transmit. If fault have not happened, the SPIFFTX.BIT.TXFFST would be change from 0 to 4 in loop and data could send successfully.
So, do you have some idea?
Waiting for yours, best wishes,
coke.