Part Number: TMS320F28335
Hi team,
Customer has some question.
1) Firstly, I am having trouble exporting my application v3 project to a stand alone app. I have followed the directions shown in the following link dev.ti.com/.../deploying.html . However, I am currently running on a windows device (and I have the windows runtime installed) but the OS_start file after exporting project as a stand-alone app is 'mac_start' and will not open on my device. Why would this be the case?
I attempted to export on a mac due to this issue (with the mac runtime installed). This does not spit any errors when attempting to open the file, but it also does not open the file, nothing happens.
2) Secondly, can you run the GUI app from the online platform, in real-time as to see values and instruments refreshing when connected to the target? (This is for both app v2 and v3).
3) Finally, for v3 specifically, the project connects to target and load firmware successfully. However, when the same project is exported as a CCS Desktop View, the following error occurs: "Error: Failed to connect: unexpected token < in JSON at position 0".
Could you help?
Best Regards,
Jiahui