Part Number: TMS320F28384D
Hi
The duty of the PWM signal must be zero, but a full duty occurs.
The program code does not allow more than 95% of duty to occur, but it does occur 100%.
Occurs at random. What's the reason?

The following is the application information:
*Solar Inverter 33kw
input: 650V
output : 220Vac 33KW
Thanks