Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
Dear TI expert,
I have alittle confuse about I2C interrupt and TX FIFO.
At TRM section 23.4.1 said, I2C general interrupt has 7 different source all ORed together.
| I2C Interrupt Request | Interrupt Source |
| XRDYINT | Transmit ready condition: The data transmit register (I2CDXR) is ready to accept new data because the previous data has been copied from I2CDXR to the transmit shift register (I2CXSR). As an alternative to using XRDYINT, the CPU can poll the XRDY bit of the status register, I2CSTR. XRDYINT should not be used when in FIFO mode. Use the FIFO interrupts instead. |
| RRDYINT | Receive ready condition: The data receive register (I2CDRR) is ready to be read because data has been copied from the receive shift register (I2CRSR) to I2CDRR. As an alternative to using RRDYINT, the CPU can poll the RRDY bit of I2CSTR. RRDYINT should not be used when in FIFO mode. Use the FIFO interrupts instead. |
| ARDYINT | Register-access ready condition: The I2C module registers are ready to be accessed because the previously programmed address, data, and command values have been used. The specific events that generate ARDYINT are the same events that set the ARDY bit of I2CSTR. As an alternative to using ARDYINT, the CPU can poll the ARDY bit. |
| NACKINT | No-acknowledgment condition: The I2C module is configured as a master-transmitter and did not received acknowledgment from the slave-receiver. As an alternative to using NACKINT, the CPU can poll the NACK bit of I2CSTR |
| ARBLINT | Arbitration-lost condition: The I2C module has lost an arbitration contest with another master-transmitter. As an alternative to using ARBLINT, the CPU can poll the ARBL bit of I2CSTR. |
| SCDINT | Stop condition detected: A STOP condition was detected on the I2C bus. As an alternative to using SCDINT, the CPU can poll the SCD bit of the status register, I2CSTR. |
| AASINT | Addressed as slave condition: The I2C has been addressed as a slave device by another master on the I2C bus. As an alternative to using AASINT, the CPU can poll the AAS bit of the status register, I2CSTR. |
I want more detail about ARDYINT and AASINT here.
First is Register-access ready condition (ARDYINT)
Assume using I2C under master transmit mode, is register-access ready condition happened when all data, which include start condition, address+read/write bit, data, and stop condition, all transmitted, so I can modify the I2C register safely? Or just simple mean all the I2C register (I2CSTR, I2CCNT ..etc.) can be access, but not mean all data had transfered?
I'm wondering this because I'm reviewing the library file "12cLib_FIFO_master_interrupt.c" in "I2c_ex6_eeprom_interrupt.c" Line 275
part of them is as below, I want to clearify the ueage of this interrupt to change master from transmitter mode into received mode.
case I2C_INTSRC_REG_ACCESS_RDY:
I2C_disableInterrupt(base, I2C_INT_REG_ACCESS_RDY);
I2C_disableInterrupt(base, I2C_INT_TXFF);
I2C_disableFIFO(base);
I2C_enableFIFO(base);
I2C_setConfig(base, (I2C_MASTER_RECEIVE_MODE));
I2C_clearInterruptStatus(base, I2C_INT_TXFF);
if(I2C_Params->numofSixteenByte)
{
I2C_setFIFOInterruptLevel(base, I2C_FIFO_TXEMPTY, I2C_FIFO_RXFULL);
}
else
{
I2C_setFIFOInterruptLevel(base, I2C_FIFO_TXEMPTY, (I2C_RxFIFOLevel)I2C_Params->remainingBytes);
}
I2C_setDataCount(base, I2C_Params->NumOfDataBytes);
I2C_sendStartCondition(base);
I2C_sendStopCondition(base);
break;
Another is about Addressed as slave condition (AASINT)
Is this interrupt be generate only when I2C under slave mode or even it is master mode?
Is this interrupt can detect the ACK from specific address of slave?
In the same file above, the code change the role from slave transmitter to slave receiver (or vice versa?)
case I2C_INTSRC_ADDR_SLAVE:
//Set TX / RX FIFO Level
I2C_setFIFOInterruptLevel(base, I2C_FIFO_TXEMPTY, (I2C_RxFIFOLevel)(I2C_Params->NumOfAddrBytes));
if((I2C_getStatus(base) & I2C_STS_SLAVE_DIR))
{
//Slave Transmitter (SDIR = 1)
I2C_setConfig(base, I2C_SLAVE_SEND_MODE);
//Enable TX FIFO interrupt and disable RXFF interrupt
I2C_enableInterrupt(base, I2C_INT_TXFF);
I2C_disableInterrupt(base, I2C_INT_RXFF);
I2C_clearInterruptStatus(base, (I2C_INT_TXFF|I2C_INT_RXFF));
}
else
{
//Slave Receiver (SDIR = 0)
I2C_setConfig(base, I2C_SLAVE_RECEIVE_MODE);
//Fill dummy data in Transmit FIFO to clear pending FIFO interrupt flag
//I2C_putData(base, 0xAA);
//I2C_putData(base, 0x55);
//Enable RX FIFO interrupt and disable TXFF interrupt
I2C_disableInterrupt(base, I2C_INT_TXFF);
I2C_enableInterrupt(base, I2C_INT_RXFF);
I2C_clearInterruptStatus(base, (I2C_INT_TXFF|I2C_INT_RXFF));
}
break;
Additional question is about the mechanism of I2C FIFO transmission:
Assuming I2C in master transmit mode, and using i2c library provided by C2000Ware 4.02.00 \ driverlib \ i2c.c
I want to put data into I2C TX FIFO using I2C_putData(), and set FIFO level to 3, and also data counter I2CCNT = 3.
Before I2C_sendStartCondition(base) being operated, the data should keep inside the FIFO, or it will shiftout when I put the data into the TX buffer?
Is this mechanism same as I2C_sendStopCondition(base) ?
If I operate I2C_sendStartCondition(base) and immediately do I2C_sendStopCondition(base),
the I2C module will transmit: start condition, address+read/write bit, data, data, data, stop condition, is that right?
Though I still have question about I2C role change, but I think that is another topic.
Thanks for your help and hope my question can help others.