Part Number: TMS320F28376S
Dear Sir ,
1. We are developing controller based on 28376S
2. The Software has two components , main loop and ISR based on XINT2
3. in some case we need to replace the source of interrupt (instead of XINT2 to be EPWM_INT)
the Switch itself should happen inside the ISR , but issue as i understand that the C28X does context save and restore (when entering and exiting the ISR)
so if i would like to Update IER inside ISR it will be overwrite once exiting ISR (context restore) , is there work around it ?