Part Number: TIDM-1000
Hi Team,
The load is 110 Ohm. The voltage is 400V.
The current loop of BUILD2 can not work when ClearTrip=1. And boost rectification operation cannot be achieved.
Is it because the load is too low?
--
Thanks & Regards,
Yale Li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDM-1000
Hi Team,
The load is 110 Ohm. The voltage is 400V.
The current loop of BUILD2 can not work when ClearTrip=1. And boost rectification operation cannot be achieved.
Is it because the load is too low?
--
Thanks & Regards,
Yale Li
Addition from customer:
I give the AC input phase voltage 50v Rms, the rectified stable voltage is 400V, and the load value is 110 ohms. After building Build2 and clearing the trip ClearTrip=1, the current loop boost cannot reach 400V.
And,
I give the AC input phase voltage 50v Rms, the rectified stable voltage is 400V, and the load value is 500 ohms, and Build2 boosts normally after clearing the trip.
What is the reason?
--
Thanks & Regards,
Yale Li
Hi Yale,
pls follow the test procedure in the user guide. Looks like it can work normally with 500 ohms.
Customer can check if the TZFLG.OST has been set. I guess it may trigger the protection for some reason.
Regards,
Chen