Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am trying to boot CPU 2(core 2) for that i am following the below steps
CPU 1(core 1) CODE :
1) configuring the IPCBOOTMODE.
2) setting flag 0.
3) bringing out CPU 2 from reset.
CPU 2 (core 2)CODE :
1) waiting for the CPU 1 ipc flag.
2) acknowledge the CPU 1.
When I flash CPU 1 code it is working fine without CPU 2 code flashing, when I flash CPU 1 code with CPU 2 activation and CPU 2 code flash CPU 1 is getting into suspend state. for this what may be the reason. am i following correct way or not? for your reference i am attaching one file.

please help me in this regards
Thanks & Regards,
k.aravind,
9848992750