This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: Send the Boot Data to M-Boot ROM using the LM Flash Programr

Part Number: F28M35H52C


Hi team,

Here's an issue from the customer may need your help:

Send the Boot Data to M-Boot ROM using the LM Flash Programr according to the app note, but the connection fails as shown in the following figure:

The development board has set the boot mode to netport boot, but the connection is not working. Is it due to incorrect setting of parameters such as IP address? Since the board was started from the network interface, what is the address?

Could you help check this case? Thanks.

Best Regards,

Cherry