This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

hardware initialization

Other Parts Discussed in Thread: TMS320F2812

Hi!

I'm using the MSK2812  board,with TMS320F2812,from Technosoft Motion.I want to use this board with Universal Converter 3 x 230 V from Leybold Didactic.

Here is the datasheet : http://www.ld-didactic.de/ga/7/735/735297/735297de.pdf

I designed the cable needed to connect this board with the converter but the converter won't start . I understand I need to create a routine to be called from the main function, but here I'm stuck.

I would appreciate any help you could give.Perhaps some .C code example or something.

Thank you,

Mihai