Hi Experts,
Good day! We need your help for our customer.
I am looking for protection relay microcontroller. I believe that you are you aware of protection power system protection. I am looking for DSP based micro controller which can take sampled values of voltage & current.
It will take sampled values analog value of current and voltages and then based on algorithm it will perform calculation & give out put its a digital signal processing based kit. It will get signals in 5 V to 24 V max.
Sampled values of current and voltages are input to the controller do you have any digital signal processing based microcontroller
I have attached it here
https://www.ti.com/lit/an/slaa466a/slaa466a.pdf the report is okay can you check the figure 3. Instead of DFT, I want to use my algorithm.
Thank you in advance.