Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am trying to use example code from below path
C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2838x\examples\c28x_dual\led, I am using XDS100v3 JTAG to flash the code. And working on CCS version 10.3.1
1) When i am flashing the CPU 1 code it is running fine, but when i try to flash the CPU 2 code it is directly going to disassembly file showing that CPU 1 is suspended at 0x3FD2AE and CPU 2 suspended due to SW break point, when i give the full run the device is getting reset. and the console is showing " Device is held in reset : take the device out of rest."
As it is a example code i am expecting no issues, can someone please help me.
Thanks & Regards
k.Aravind,
9848992750.