This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Disconnection during parameter identification

Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: BOOSTXL-3PHGANINV, , LVSERVOMTR, MOTORWARE

I am currently trying to run the default motor, LVSERVOMTR, using LAUNCHXL-F28069M and BOOSTXL-3PhGanInv Evaluation Module.
I ran lab2a using the BOOSTXL-3PhGanInv Evaluation Module manual and the motorware manual as reference and found that "gMotorVars.Flag_enableSys" and "gMotorVars.Flag_Run_Identify Flag_Run_Identify" to 1, the motor rotates, but an error occurs in the process, as shown in the attached image.


Once I was able to control the speed without the error, but after that, the same error occurs.
I think the hardware connection is correct.
What can be possible cause of this issue?