Part Number: TMS320F28375D
Hi.
I am working with tms28375d microcontroller. I am trying to use 200MHz system clocking, however i am running into problem when i am trying to run the code on CPU. I am getting the following error if i try to set exactly 200MHz frequency. 
I am using the libraby provided function InitSysPLL with the following settings. My External clock frequency is 20Mhz.
After reading the datasheet I've noticed that in some examples the frequency wasn't eactly set to 100MHz, but a slightly smaller value? Why? Should i also use a slighly smaller value for 200Mhz clock? Is it possible to set exactly 200Mhz clock?
Thank you for your responce.
Best regards.