This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Abnormalities of ADC sampling spike

Part Number: TMS320F280049C

Hi Team,

I have encountered some problems when using ADC.

The figure below shows the waveform of the measurement, where Iout refers to the output current, obc_curr_adc is the signal entering the DSP, and DAC_obc_curr_adc is the value directly converted from the obc_curr_adc pin, which is generated by the DAC, and the DAC output interval time, the same as the ADC value, stands at 50us(20kHz).

It can be observed that the DAC output maintains a spike at an interval, but at the same time the signal entering the DSP does not achieve a spike. When testing other ADC pins, the same situation exists. I would like to know what may have caused the problem, thank you.

Kind regards,

Katherine