Other Parts Discussed in Thread: TMS320F280039, C2000WARE
Hi There,
MY INPUTS / PLANS
I am preparing to generate a Sine Wave as output from DSP to get converted via DAC as final output.
The output pins on DSP are being planned as below as Input to DAC
MCLKXA --- DAC_SCLKMDXA --- DAC_SDI
MFXA --- DAC_/LOAD
The DAC will finally generate a Sine Wave Output.
The input to DSP as variable is from a serial pulse output from a rotating device which generates a PULSE output.
MY QUERY:
I am new comer to CCS. In order to quickly program a CCS.....
Which Launchpad is best suitable with examples to generate a Sine Wave for above INPUTS?
Plz share the code to generate a Sine Wave output to control the rate of amplitude, angle, frequency from a serial input containg the pulse output.