This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 byte = 16 bits questions.

Hello, 

I have few questions, all related to the "byte = 2 bytes " phenomenon of the C2000:

1. Will memory work as expected when I copy non even size of bytes ? (or simply last argument will be in-effect twice as large ?)

2. Will printf by able to access 27 bytes in RAM and print them (that last byte is NULL) in this example.

3 What will strlen() return for "C2000" ?

4. Can I define a pack(1) struct ?

5. How can I preform  CRC32 on an odd size of memory region?

6. Is there a salsa20 implementation for this MCU?

6. Can I define struct with bit-fields ?

7. Can I read /write single byte to/from SPI / UART (I know there is a difrent name for UART, cause why use something from the mid 60's?)

8. How can I create a packed struct with odd size (count of bytes) of elements, for ex:  ?

While at it, how can I access 'b' assuming b is a uint8_t (one byte ), without the ugly _byte() intrinsic ?

struct my_struct {

    char a[3];
    bool b;
    char c[3];
};

9. What will memcmp() return for : { 0xa5,0xa7,0xa3 } and  { 0xa5,0xa7,0xa3, 0x00 } ?

Thanks,

Eitan Michaelson,

SolarEdge, Israel.