Part Number: TMS320F28027
Hi,
Good Day.
The customer is using TMS320F28027. He wants to increase the CPU speed to execute code faster. When CPU speed is 10MHz, the profile clock between a breakpoint is about 18000, when CPU speed is 20MHz, the profile clock is 40000, mean profile clock increased when CPU speed increased and execution time increased. Code is executed from flash, wait state is set to 1. He doesn’t know why execution time increases.
Please advise. Thank you very much.
Best Regards,
Ray Vincent