Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE
Hello, TI Experts,
In my application, I guess I likely need 6 or 7 ePWM(A/B) pairs[see my attached PWM output waveforms]. I'm trying to figure out whether I can realize this from LAUNCHXL-F280049C LAUNCHPAD. Therefore, I'm planning to combine epwm_ex2_updown_aq.c and epwm_ex3_synchronization.c(if needed) from C:/ti/c2000/C2000Ware_4_02_00_00/driverlib/f28004x/examples/epwm/CCS.


Questions:
1. Can I generate the simulated PWM outputs with this Launchpad with ePWM1,2,3,4,5,6,8 (i dont see ePWM7)?


2. In epwm_ex2_updown_aq.c default program, do EPWM1A and EPWM1B naturally complementary like it's in PWM waveform inverter picture? If not, how to make them 180 deg phase shifts.
3. I'm planning to activate EPWM4,5,6,8 in epwm_ex2_upddown_aq.c by adding[
(correct me if i'm wrong) it looks like the EPWM1,2,3,4 are 90 deg phase shift in order per comments from epwm_ex3_syn. Does it mean the EPWM5 has the same phase with EPWM1, EPWM6 has the same phase with EPWM2, AND EPWM8 has the same phase with EPWM4? If so, then, I might need to adjust the phase shift values for EPWM5,6,8. Sounds like we have to modify the EPWM_setPhaseShfit () function or define phasecount value, but I'm not sure how to do it? Any comments will be very helpful!