This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: the size of out file .bin is bigger than .hex

Part Number: TMS320F28035


Hi Team,

Here's an issue from the customer may need your help:

CCS12.1.0

Under normal circumstances, the Bin file of the same project should be smaller than Hex.

But the .bin file the customer generated is 128K, The .hex file is only 45K.

--

Thanks & Regards,

Yale Li