Part Number: TMS320F280023
Hello,
I want to use Input X-Bar as eCAP. In this case, I have to select an input X-Bar for eCAP, so it can be configured with ECCTL0 [INPUTSEL] register.
However, the select index in Table 18-1 seems different. In the case of 280049, it shows the input X-Bar selection for eCAP as in Table 19-1.
Can I use the input select register for 280023 like 280049?
Also, if I want to used AIO pin for eCAP, how do I select input for eCAP. It is difficult to find the correct selection register.