Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
Hi team,
I am very new to TMS320F280025c microcontroller. In my project I wanted to use LIN communication in SCI mode with DMA and wanted to view the data bytes in putty terminal.
The program I found from the example code of "C2000Ware_4_02_00_00\driverlib\f28002x\examples\lin\lin_ex3_sci_dma.c "
I found that GPIO_22 and GPIO_23 pins are used for LIN_tx and LIN_rx respectively. So, I configure those pins and disable the internal loopback mode. For the transmission, I only sent two bytes of char data and did some modifications. In oscilloscope, I observed a single pulse is being triggered via GPIO_22 pin after a DMA transmission request but didn't find any data bits or other pulses.
The modified code, I am attaching herewith. Your help would relief me out of the burden. Please help me out.
//#############################################################################
//
// FILE: lin_ex3_sci_dma.c
//
// TITLE: LIN SCI MODE Internal Loopback with DMA
//
//! \addtogroup driver_example_list
//! <h1> LIN SCI MODE Internal Loopback with DMA </h1>
//!
//! This example configures the LIN module in SCI mode for internal loopback
//! with the use of the DMA. The LIN module performs as SCI with a set
//! character and frame length in multi-buffer mode. When the transmit buffers
//! in the LINTD0 and LINTD1 registers have enough space, the DMA will transfer
//! data from global variable sData into those transmit registers. Once the
//! received buffers in the LINRD0 and LINRD1 registers contain data,the DMA
//! will transfer the data into the global variable rdata.
//!
//! When all data has been placed into rData, a check of the validity of the
//! data will be performed in one of the DMA channels' ISRs.
//!
//! \b External \b Connections \n
//! - None
//!
//! \b Watch \b Variables \n
//! - \b sData - Data to send
//! - \b rData - Received data
//!
//
//#############################################################################
//
//
// $Copyright:
// Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Defines
//
//Modified
// #define BURST 4
// #define TRANSFER 32
// #define CHAR_LENGTH 8
// #define FRAME_LENGTH 8
#define BURST 1
#define TRANSFER 1
#define CHAR_LENGTH 8
#define FRAME_LENGTH 1
//
// Configure the Baud Rate to 115.207kHz
//
uint32_t PRESCALER=0x000001a;
uint16_t DIVIDER=0x0002;
//
// Globals
//
//Modified
uint16_t sData[2] = {'a', 'b'};
uint16_t rData[2];
// unsigned char *sData;
// unsigned char *rData;
//Place buffers in GSRAM
#pragma DATA_SECTION(sData, "ramgs0");
#pragma DATA_SECTION(rData, "ramgs0");
volatile uint16_t done = 0; // Flag to set when all data transfered
//
// Function Prototypes
//
void initDMA(void);
void configureSCIMode(void);
__interrupt void dmaCh5ISR(void);
__interrupt void dmaCh6ISR(void);
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
//
Device_init();
//
// Initialize GPIO
//
Device_initGPIO();
// Pin config for LIN tx and LIN rx
GPIO_setPinConfig(DEVICE_GPIO_CFG_LINTXA);
GPIO_setPinConfig(DEVICE_GPIO_CFG_LINRXA);
// GPIO_23 is used as LINTXA
GPIO_setDirectionMode(23, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(23, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(23, GPIO_QUAL_ASYNC);
// GPIO_23 is used as LINRXA
GPIO_setDirectionMode(22, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(22, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(22, GPIO_QUAL_ASYNC);
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
EINT;
ERTM;
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
// This registers the interrupt handler in PIE vector table.
//
Interrupt_register(INT_DMA_CH5, &dmaCh5ISR);
Interrupt_register(INT_DMA_CH6, &dmaCh6ISR);
//
// Enable the DMA interrupt signals
//
Interrupt_enable(INT_DMA_CH5);
Interrupt_enable(INT_DMA_CH6);
//
// Initialize the DMA
//
initDMA();
//
//Initialize the LIN Module
//
LIN_initModule(LINA_BASE);
//
// Configure the LIN module to operate in SCI mode
//
configureSCIMode();
//
// Initialize the data buffers
//
//Modified
// for(i = 0; i < 128; i++)
// {
// sData[i]= i;
// rData[i]= 0;
// }
//
// Wait for the SCI receiver to be idle
//
while(!LIN_isSCIReceiverIdle(LINA_BASE));
//
// Wait until space is available in the transmit buffer.
//
while(!LIN_isSCISpaceAvailable(LINA_BASE)){}
//
//Initiate transfer through a CPU write
//
LIN_sendData(LINA_BASE,(unsigned int*)0xFFFF);
//
// Start the DMA receive channel
//
DMA_startChannel(DMA_CH6_BASE);
//
//Start the DMA transmit channel
//
DMA_startChannel(DMA_CH5_BASE);
//Write one data byte when Tx buffer is ready
LIN_writeSCICharBlocking(LINA_BASE, sData[1]);
//
//Wait until the DMA transfer is complete
//
// while(!done);
//
//When the DMA transfer is complete the program will stop here
//
ESTOP0;
}
//
// Function to configure LIN in SCI Mode
//
void
configureSCIMode(void)
{
//
// Enter LIN reset state to perform configurations
//
LIN_enterSoftwareReset(LINA_BASE);
//
// Switch LIN into SCI mode
//
LIN_enableSCIMode(LINA_BASE);
//
// Set the SCI communication mode to idle line
//
LIN_setSCICommMode(LINA_BASE, LIN_COMM_SCI_IDLELINE);
//
// Set SCI to transmit one stop bit
//
LIN_setSCIStopBits(LINA_BASE,LIN_SCI_STOP_ONE);
//
// Disable parity check
//
LIN_disableSCIParity(LINA_BASE);
//Modified
//
// Enable multi-buffer mode
//
// LIN_enableMultibufferMode(LINA_BASE);
//
// Module set to complete operations when halted by debugger
//
LIN_setDebugSuspendMode(LINA_BASE, LIN_DEBUG_COMPLETE);
//
// Set character length as 8-bits
//
LIN_setSCICharLength(LINA_BASE, CHAR_LENGTH);
//
// Set to 1 character in response field
//
LIN_setSCIFrameLength(LINA_BASE, FRAME_LENGTH);
//
// Set the Baud Rate
//
LIN_setBaudRatePrescaler(LINA_BASE, PRESCALER, DIVIDER);
//Modified
//
// Enable Internal Loopback mode
//
// LIN_enableIntLoopback(LINA_BASE);
// LIN_disableIntLoopback(LINA_BASE);
//
//Enable the DMA for transmission
//
LIN_enableSCIInterrupt(LINA_BASE, LIN_SCI_INT_TX_DMA);
//
//Enable the DMA to receive
//
LIN_enableSCIInterrupt(LINA_BASE, LIN_SCI_INT_RX_DMA);
// Exit LIN reset state
//
LIN_exitSoftwareReset(LINA_BASE);
}
//
// DMA setup for both TX and RX channels.
//
void initDMA()
{
//
// Initialize DMA
//
DMA_initController();
//
// Configure DMA Ch5 for TX. When there is enough space in the buffers found in
// the LINTD0 and LINTD1 registers, data will be transferred from the sdata buffer
// to the LIN's transmit registers. The destination address is configured to start
// in the most significant part of the LINTD1 register (TD4/TD5 transmit buffers)and
// move two address's down with every burst until it fills up the least significant
// part of the LINTD0 register (TD2/ TD3 transmit buffers).After every transfer of
// 4 bursts the destination address is brought back to the address of the TD4/TD5
// buffers contained in the LINTD1 register.
//
//Modified
// DMA_configAddresses(DMA_CH5_BASE, (uint16_t *)(LINA_BASE + LIN_O_TD1+2), sData);
// DMA_configBurst(DMA_CH5_BASE, BURST, 1, -2);
// DMA_configTransfer(DMA_CH5_BASE, TRANSFER, 1, 6);
// DMA_configMode(DMA_CH5_BASE, DMA_TRIGGER_LINATX, DMA_CFG_ONESHOT_DISABLE |
// DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT);
DMA_configAddresses(DMA_CH5_BASE, (uint16_t *)(LINA_BASE + LIN_O_SCITD), sData);
DMA_configBurst(DMA_CH5_BASE, BURST, 0, 0);
DMA_configTransfer(DMA_CH5_BASE, TRANSFER, 0, 0);
DMA_configMode(DMA_CH5_BASE, DMA_TRIGGER_LINATX, DMA_CFG_ONESHOT_DISABLE |
DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT);
//
// Configure DMA Ch5 interrupts
//
DMA_setInterruptMode(DMA_CH5_BASE, DMA_INT_AT_END);
DMA_enableInterrupt(DMA_CH5_BASE);
DMA_enableTrigger(DMA_CH5_BASE);
//
// Configure DMA Ch6 for RX. When the buffers found in the LINRD0 and LINRD1
// registers are full, data will be transferred to the rdata buffer. The source
// address is configured to start in the most significant part of the LINRD1
// register (RD4/RD5 receive buffers) and move two address's down with every
// burst until it transfers the least significant part of the LINTD0 register
// (RD2/ RD3 receive buffers).After every transfer of 4 bursts the source
// address is brought back to the address of the RD4/RD5 buffers contained in
// the LINRD1 register.
//
//Modified
// DMA_configAddresses(DMA_CH6_BASE, rData,(uint16_t *)(LINA_BASE + LIN_O_RD1+2));
// DMA_configBurst(DMA_CH6_BASE, BURST, -2, 1);
// DMA_configTransfer(DMA_CH6_BASE, TRANSFER, 6, 1);
// DMA_configMode(DMA_CH6_BASE, DMA_TRIGGER_LINARX, DMA_CFG_ONESHOT_DISABLE |
// DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT);
DMA_configAddresses(DMA_CH6_BASE, rData,(uint16_t *)(LIN_O_SCIRD));
DMA_configBurst(DMA_CH6_BASE, BURST, 0, 0);
DMA_configTransfer(DMA_CH6_BASE, TRANSFER, 0, 0);
DMA_configMode(DMA_CH6_BASE, DMA_TRIGGER_LINARX, DMA_CFG_ONESHOT_DISABLE |
DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT);
//
// Configure DMA Ch6 interrupts
//
DMA_setInterruptMode(DMA_CH6_BASE, DMA_INT_AT_END);
DMA_enableInterrupt(DMA_CH6_BASE);
DMA_enableTrigger(DMA_CH6_BASE);
}
//
// DMA Channel 5 ISR
//
__interrupt void dmaCh5ISR(void)
{
DMA_stopChannel(DMA_CH5_BASE);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);
return;
// done = 1;
}
//
// DMA Channel 6 ISR
//
__interrupt void dmaCh6ISR(void)
{
uint16_t i;
DMA_stopChannel(DMA_CH6_BASE);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);
//Modified
// //
// //Check for data integrity
// //
// for(i=0; i<128; i++)
// {
// if(rData[i] !=i)
// {
// //Something went wrong, rdata doesn't contain expected data.
// ESTOP0;
// }
// }
// done = 1;
return;
}




'