Part Number: TMS320F28069
Hi
I was not able to program the flash in 28069 launchpad using the example projects within the C2000 ware. I have some old projects based on
28069, created in CCS version 6, where I was able to program the flash. But I'm unable to use that in the Version 11 as i'm getting an error
"This project was created using a version of compiler that is not currently installed - 6.1.1 [C2000]. "
Kindly help resolve
1. Either to use the old project
2. Or to use the example projects in C2000 ware to load the flash..
Thanks
Lenin.