Part Number: TMS320F28377D
Hello,
I'am working on a complex project using both CPU1 and CPU2 to control a DC/DC converter.
CPU1 is dedicated to regulation, whereas CPU2 is dedicated to communication with other parts of the system.
To increase even more regulation period execution, I decided to transfer the code for my regulation on the CLA of CPU1.
By doing this, I had to rewrite my drivers (PWM) to allow compilation for CLA. It forced me to change the CMD file of both processors to define CLA sections (code and program).
As LSRAM was used to execute TI functions (including CRC), they were not enough space in this RAM to place CLA and code and program.
So, I had to map TI functions, .ebss .esysmem and .cio in the GSRAM. After doing this, I observed an execution problem on the CPU2 when debugging.
During initialization, I use the VCU CRC module and it goes in Illegal ISR interrupt.
The same code was perfectly working before.
Could you please help me with this issue ?
I can provide only small part of source code for confidentiality.
Thank you,
Arthur