Part Number: TMS320F28022-Q1
Hi BU experts,
Customer found one board with RAM error. They modified the RAM at address of 0x400 via emulator memory browser (the value is changed from 0x0000 to 0xAAAA), but some other RAM bytes after this address, such as 0x402, 0x414 etc., their value will change to 0x0020 too. And some address such 0x404, some bit can't be changed to 1 (write 0xAAAA, but actually store 0xAA8A).
Only M1 RAM has this problem, M0 and L0 don't show this error.
Please help check if this kind of problem be found before, the root cause and possible workaround.
Thanks & Regards,
Will