Part Number: TMS320F28377S
Hi Team,
Here are some issues from the customer may need your help:
ADC configurations:

(This is the configurations that after fixed issue 2.)
EPWM configurations:


EPWM1 ISR:

EPWM2 ISR:

issue:
1. The relevant ADC sampling value will appear issue shown below during EPWM2 interrupt:

(The value in AdcaResultRegs.ADCRESULT2 mutated to 0.)
2. The green waveform represent the value of AdcaResultRegs.ADCRESULT7. The sampling is selected by emulation switch from 2 sampling channels. The sampling is not coupled after exchange AdcaResultRegs.ADCRESULT0 and AdcaResultRegs.ADCRESULT7. It seems like the channels of Group A are influenced by the conversion time. The conclusion from the customer is that more important sampling should be configured as former as possible. So he'd like to know are there any cautions about it?

--
Thanks & Regards,
Yale Li