Part Number: TMS320F28377S
Hi Team,
is below issue is with gel file? i'm working on TMS320F28377S processor and from dss java script i'm trying to keep breakpoint for end of the execution(exit.c).
ErrorLog:
Begin scripting session
Connecting the Target
Target Connected
WARNING: C28xx_CPU1_0: Breakpoint Manager: Retrying with a AET breakpoint
Loading the Program
Executing the Program
WARNING: C28xx_CPU1_0: Breakpoint Manager: Retrying with a AET breakpoint
SEVERE: C28xx_CPU1_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x85d58: (Error -1066 @ 0x85D58) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.4.0.00129)
SEVERE: C28xx_CPU1_0: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x85dba: (Error -1066 @ 0x85DBA) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.4.0.00129)
End scripting session