Part Number: TMS320F28379D
Hello,
I have a problem when I'm using _DUAL_HEADERS predefined symbol,
When I use the ADC, ADC_RESOLUTION_12BIT macro is not defined and instead ADC_BITRESOLUTION_12BIT is defined,
but in the function {AdcSetMode((uint16_T)ADC_ADCC, (uint16_T)ADC_RESOLUTION_12BIT,(uint16_T)
ADC_SIGNALMODE_SINGLE); } when I'm generating the code from Simulink it use ADC_RESOLUTION_12BIT and I should change it manually to make it works.
I want to see if you have a solution to this problem?