Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Hi i am using sci_ex3_echoback example code. Please answer some my questions.
1 . By default code is saving it RAM , then the code is working , but when i selected the flash for the program in ccs option, the program take long time to saving controller and does not work, why is it so?
2. When i am pressing the reset button on the eval board or power on off the board the program is not restarting , why is it so and how can i correct this ?
3. How can i increase the size of ram for the program and how can in increase the size of the flash for the program, because when am adding other peripherals in the code and code size is keep increases , it show error and indicate RAM is Overlapping with other section of the RAM.
kindly help with this .