All,

The first revision of the Concerto F28M35x Technical Reference manual (SPRUH22) is on the web.

http://www.ti.com/litv/pdf/spruh22

Note that this is a preliminary revision of the reference manual - it is still missing the following chapters (to be released end of July/Aug):

  • System Control and Interrupts
  • Inter-Processor Communications (IPC)
  • Internal memory (Flash/RAM)
  • Boot ROM - release in Aug.
  • Enhanced Pulse-Width Modulator (EPWM) - release in Aug.
  • High-Resolution PWM (HRPWM) - release in Aug.
  • Analog (ADC + COMP)
  • GPIO's
  • C28 DMA
  • M3 SSI
  • M3 UART
  • Cortex-M3 Processor
  • Cortex-M3 Peripherals