Part Number: TMS320F28069F
Dear Yanming Luo:
I am conducting sensor FOC control experiment. The motor is IPMSM. I refer to the existing thread in the forum:
e2e.ti.com/.../tms320f28069m-encoder-feedback-angle-isn-t-right-when-running-lab12b ,
but I need your help when I encounter problems.
1. Is it normal for the motor speed to rise to the maximum speed very quickly when the rotor position calibration is incorrect?
2. I use the above thread scheme to obtain Angle_est from sensorless control mode when the motor rotates forward for 2s, and complete offset calibration (Counter=angle_est * 4 * encoder_line/(2 ^ 24)/Pole_ Pairs), and switch to the sensor control mode at the same time, which is very good. However, the same method is used to perform offset calibration when the motor is running in reverse direction. The calibration fails and the motor has Q1 phenomenon. How can the motor run in reverse from the obtained Angle_ est calculates the count value?
Regards
Quan